Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
5.8. Table layout for
PARTdataManager and (PARTlinkManager)
5.8.1. Tabellenwerte anpassen
-> Text anpassen / plinkcommon.cfg -> Block
[MAPPING_<COLUMN_NAME>] - Key for visible text
|
|
---|---|
Zurück | Weiter |
With the help of the option Text anpassen you can set text to be displayed in the standard color "black".
The setting applies for PARTdataManager and PARTlinkManager as well.
Setting in
configuration
file $CADENAS_SETUP/plinkcommon.cfg
:
Block [MAPPING_<variable name>], key name is the displayed text, value is the internal value.
[MAPPING_ACTIVE_STATE] Locked="0" Released="1" Expired="2"
[MAPPING_ACTIVE_STATE] 0="0" 1="1" 2="2"
Setting in user interface under PARTlinkManager -> Extras menu -> Konfigurieren dialog box -> PARTlinkManager Einstellungen tab -> Tabellenwerte anpassen -> Text anpassen:
Exampe for ACTIVE_STATE: The internal values stand for locked (0), released (1) und expired (2). The respective visible value is displayed in black color.
Zurück | Nach oben | Weiter |
5.8. Table layout for PARTdataManager and (PARTlinkManager) | Zum Anfang | 5.8.2. Tabellenwerte anpassen -> Farbe anpassen / plinkcommon.cfg -> Block [COLMAPPING_<variable name>] - Key COLORCODE<Nummer> |