Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The installation of Apache version 2.2 is needed to provide static content faster.
Default port number for APACHE inside DMZ is 80. Port number can be changed by Sysadmin.
The JBoss will be connected to the Apache later to secure the management console.
Hinweis | |
---|---|
If the JKConnector is used, only the Apache server has to be accessible through port 80. No other ports are needed from outside to access the system. |
The APACHE Webserver alternatively can also be installed in the "INTERNAL" area (instead of DMZ area), if a REVERSE PROXY is installed inside the DMZ.
Zurück | Nach oben | Weiter |
4.3.5. Apache 2.2 | Zum Anfang | 4.3.5.2. 3. Specific installation steps |