Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
1.1.6.10.1. Tweakmenu: Adjust
menus, menu items, toolbars, icons and context menu commands
1.1.6.10.1.4. Special
settings in partsolu.cfg
|
|
---|---|
Zurück | Weiter |
With the help of the key sortToolbars under $CADENAS_DEFAULT_USER -> block [TWEAKMENU] the position of the toolbars is saved. When restarting the application the set positions are recovered.
toolbarOrderTop=Standard,Assembly,Details,Export,\n,Views,LinkDatabase,Addsap,IndexTree
The value of the config key will be set to 0 when the application is closed.
Key PARTdataManager_Mode (or PARTproject_Mode)
The key saves the mode (Beginner / Professional) which is used when opening the application. Under Extras menu -> Mode auswählen you can switch anytime.
Add further applications to be controlled by tweak configs
If you want
to add a new application, which should be controlled by the tweakmenu
you must insert the name of the application as value of the key
processedApps in the $CADENAS_USER/partsolu.cfg
.
Of course you have to create the two configs, which are described
above. Copy the content of menustructure_PARTdataManager.cfg
and menuvisibility_PARTdataManager.cfg
to get a quick start.
Zurück | Nach oben | Weiter |
1.1.6.10.1.3. menuvisibilty-config | Zum Anfang | 1.1.6.10.1.5. Scripting with "Tweakmenu" |