Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
5.9.1. Basic design of
"Neue Ident-Nummer" dialog box - erpcustom.cfg
-> Block [USERDIALOG]
5.9.1.1. Ignore custom set values for the
combobox - Key "USERDIALOG_SKIPDBLOAD"
|
|
---|---|
Zurück | Weiter |
By default, both
the values specified in material_assign.cfg
and the custom
set values of the table are shown in the combobox list.
If you want to exclude the custom set values of the table for specified database fields, do the following:
1. USERDIALOG_SKIPDBLOAD=MAT_NAME -> The "Material" combobox is only filled with the config values. Table values are ignored.
2. USERDIALOG_SKIPDBLOAD=MAT_NAME,LOC1 -> The "Material" and the "Location 1" comboboxes are only filled with the config values. Table values are ignored.
Zurück | Nach oben | Weiter |
5.9.1. Basic design of "Neue Ident-Nummer" dialog box - erpcustom.cfg -> Block [USERDIALOG] | Zum Anfang | 5.9.2. Change default description text for ERP_PDM_NUMBER - erpcustom.cfg -> Block [VARS] -> Key "USERDIALOG_ERPNR" |