Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
![]() |
Hinweis |
---|---|
Deprecated: In order to control the visibility of buttons please use Abschnitt 1.1.6.10.1, „Tweakmenu: Adjust menus, menu items, toolbars, icons and context menu commands“. |
User interface: PARTadmin -> "Roles" category -> "Menu" tab -> Use these settings
If the checkbox Use these settings is disabled, then all buttons of the ERP toolbar are active. If not, the individual setting for each button takes effect (compare key "BUTTONS").
It controls the buttons of the ERP toolbar.
0: The individual settings are not used.
That means, all buttons of the ERP toolbar are enabled (no one grayed out).
(If the buttons is enabled in PARTlinkManager -> Extras menu -> Configure ERP environment -> PARTdataManager preferences tabbed page -> Login mode)
1: The settings for the individual buttons take effect.
(In the config file see stated buttons in the key "BUTTONS".)
Menu tabbed page: Control of the buttons in the ERP toolbar; active or grayed out.
Zurück | Nach oben | Weiter |
1.1.6.7.22.14. Key "IMAGE" - Displayed bitmap | Zum Anfang | 1.1.6.7.22.16. Key "TEMPLATE" |