Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Basically the software is made up of the 5 components listed below. All components, central or local, can be individually installed.
Per location, one PARTsolutions installation. In one location there is a master installation, which is replicated cyclically to the other installations. At this master location all updates are imported. Should performance problems arise in one location, it should theoretically be possible to install per department, although the maintenance and replication effort increases.
One central LinkDB. The LinkDB can be installed at a central location which can be easily reached by all other locations. Should the network performance not suffice, the LinkDB can be installed at every location and replicated per database mechanism. The LinkDB is independent of the database used in the company. Of course the existing database may be used for the LinkDB as well. Experience has been made with, among others, MS SQL Server, Oracle, SAPDB, mySQL.
|
The fingerprints are usually found with the catalog state and are thus also replicated with a catalog update.
Note | |
---|---|
To speed up the search, the PARTapplicationServer should be implemented for a Client-Server installation. See more information underSection 2.2.4, “PARTapplicationServer Installation”. |