Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
Setting up PARTapplicationServer as service is advantageous, because it is automatically started at start of the server and Windows mechanisms for monitoring the stability (e.g. restart at crashes) are used. (Restart delay can be adjusted via registry.)
You have the opportunity to set up the service during the PARTsolutions Server installation. Hereto simply activate the respective option.
After finished installation the service "PAPPSERVER" is displayed under Windows -> Control panel -> Administrative tools-> Services.
With the command pappserver.exe -install
[5] you can manually set up the service in a console.[6]
![]() |
Note |
---|---|
When manually setting up the service the respective administrative permissions have to be given. |
The installer sets up an UNC path for the AppServer service. Possibly this is not yet available when starting the service.
Furthermore UNC paths are slower than shares and local installation paths.