powered by CADENAS

Manual

Manual

11.5.2.4.  Sequence

In this window, you can determine in what sequence the variables are to be displayed later in the PARTdataManager table (from left to right).

The variable in the topmost row of this window is positioned at the start (far left) of the table in PARTdataManager (see illustration below).

  1. First click on the Variablewhich you wish to move.

  2. Then move it to the required position. There are alternative ways of doing this:

  • drag the variable with the mouse button pressed or

  • drag the variable by two positions in each case using the arrow button

Then confirm with OK if you agree with the sequence of all variables.

Result in PARTdataManager

Sequence from left to right