powered by CADENAS

Manual

Manual

8.5.5.  Image-table connection

Connect technical previews (*.tif or *.pra) with table-variables in the PARTdataManager:

Start PARTproject and select an image file (for example, *.pra or *.tif).

The Preview shows up.

Activate the command Define image-table-connection in the context menu of the image (right mouse button).

Pull up the connection with the left mouse button (Example: diameter B).

-> The window opens

Select the corresponding variable.

-> The connected areas are marked in blue stripes.

For later development, or to remove, the corresponding commands are now available in the context menu as well.

Results in the PARTdataManager

Save project and start PARTdataManager.

Click the diameter (B) in the Technical details window.

-> A dark-gray marking in the head of the column in the table, shows the connected variable.