powered by CADENAS

Manual

Manual

7.2.1. Opening PARTdesigner

In order to open PARTdesigner, to edit a geometry, do the following:

  1. Mark the file *.3db (or possibly *.3gb).

    -> In the Edit project dialog area the 3D preview shows up.

  2. Click on Edit.

    You have only 2 options:

    1. The file already contains content which you want to edit.

      -> PARTdesigner opens directly.

      PARTdesigner

      PARTdesigner

    2. The file does not yet contain content and you want to apply it:

      You will be asked in the Edit file window, whether or not the file *.3db file is to be applied..

      Use variable from table

      Use variable from table

      If desired, set a checkmark at the option field Use variable from tableso that the variables will be transferred to PARTeditor and confirm with OK.

[Note] Note

A detailed description of PARTdesigner can be found under Chapter 10, PARTdesigner parametric tool .