powered by CADENAS

Manual

Manual

14.3.4. "File" menu

  • New: See Section 14.3.1, “"Basic functions" toolbar”.

  • Open: The Explorer is opened with the directory "_templates". All files of the type .template are displayed.

  • Import: Templates from versions older than 9.04 use a file „Name.pdf" and a file „Name_empty.pdf" (background with images). Via Import you can import these two PDFs.

    Since PDF files cannot be converted to images, the file „Name_empty.pdf" has still to be used at an import.

    However, once a template is updated to the current format, the background PDF should be preferably replaced by respective images and so is not needed anymore.

  • Recent files:

  • Save: Saves the template in the existing .template file.

  • Save as: The Explorer is opened in the directory "_templates". All files of the type .template are displayed. Possibly save the template under a new name.

  • Exit: PARTtemplateDesigner is finished.