powered by CADENAS

Manual

Manual

4.7.2.1.11.  Sort directory

The order of the various directories / folders in the tree can be changed.

  1. Mark the directory whose subdirectories you wish to reorder.

  2. Click on tabbed page General1 -> Sorting of the directory in the Define sorting pull-down menu.

  3. Click on Sort directory in the context menu.

  4. In the Sequence dialog window, you can change the position of subdirectories by marking them and moving the arrow either up or down, or simply reposition with Drag & Drop.

  5. Confirm with OK. --> The new order is applied to the PARTproject tree.

  6. Click on Save.

[Note] Note

As of PARTsolutions V9.03 you can sort your own catalogs as well.

[Note] Note

In order for these changes to be active in PARTdataManager please carry out the following command on the respective directory level: PARTadmin -> Index administration -> Update. See Section 1.1.3.4.5.2, “Context menu commands in detail ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.

If you want to carry out the command for all catalogs, then use the Generate new search index command. See Section 1.1.3.4.4.2, “ Update search index ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.

Attention! This can, depending on the number of catalogs, possibly take hours!