Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
At directory level the menu item Set QA status has no sub-menu items.
Select the new QA status in the pull-down menu. It is possible that there is no selection available.
Note | |
---|---|
It is impossible to set up a QA status of a superior directory, if a hierarchical subordinate project / directory has a lower QA status! (see error message below) |
Using the option Set status in projects and directories a status can be set in projects and subdirectories. In this case you will not get an error message.
Using another option"Set only if the current status is", you can limit or specify the status allocation to your needs.
Note | |
---|---|
The selection of a comment in the pull-down menu is obligatory! (See also Section 6.10, “ History tab page ”) When selecting "Other" you can add any comment in the active text field. |