Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
PARTproject should insert a part into a classification, assign it an attribute, and display the result in the PARTdataManager.
Choose the corresponding directory into which the selected part should be inserted.
Note | |
---|---|
Only after an Index update in PARTadmin (see Section 1.1.3.4, “ Index administration ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual) will the result be visible in the PARTdataManager. |
A classification can be planned for parts, as well as for Connection points .
In case both options are possible, select the option Classes or Connection points before allocation in the selection list under Filter (see figure below).
The most classes only have the Classes option is available.
The Classification window can be reached via the context menu of the directory tree via Add projects to classification.
For more information see the next section under Section 5.6.2, “Allocation at directory level”.
The context menu command Add projects to classification is available at project level, as well as at directory level.