Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Places a text into the sketch view.
The "Text" element is declared with "ELEMENT_" followed by a unique identification for the element.
[ELEMENT_text1]
The following attributes are available:
Indicates stretch factor of width for text. Minimum possible value is '0.5'.
Indicates whether size/position of text element may be changed in Edit mode.
Indicates, whether the text indicated under "text", should be translated.
Here, a *.def file must be indicated, in which the translation for the texts are entered. Compare also Section 5.4.4.11, “ Translations ”.
The def file must be entered in the frame element. Compare Section 5.4.4.9, “[ELEMENT_frame] Combine more elements in frame ”.
Information on the use of Attribute algorithms is found under Section 8.5.2.7.1, “Translation functions”.
The following attributes MUST be assigned:
[ELEMENT_text1] type=text parent=frame position_x=200.00 position_y=200.30 position_w=60.00 position_h=15.00 text=Normtext: $NT. text_size=3 width_factor=0.5 sizeable=false translateable=true
[ELEMENT_text1] type=text parent=frame position_x=226.31 position_y=60.98 position_w=51.22 position_h=5.05 text=(area of use) text_size=2 width_factor=0.5 sizeable=false translateable=true
use_ratio=true text_align=left rotation=horizontal