Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Note | |
---|---|
If PARTproject QA is activated, your catalogs are under SVN administration. In this case do not use PARTupdate! More information regarding PARTupdate can be found here: Section 1.1.3.3, “ Catalog update ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual. |
Within the project selection of PARTproject, it is not necessary that catalogs be managed by SVN. By means of the symbols mentioned above both states are well-defined.
Using PARTproject QA you are working exclusively with SVN managed catalogs.
For a local working basis you must download the catalog that should be used once. You will find 23d-libs in the context menu of the directory tree under the command Download catalog from server to do this.
The following screenshots show the downloading of a catalog.
In the context menu, select Versioning system -> Download catalog from server.
In the index tree, select the desired catalog. If you have many catalogs installed use the input field in order to filter.
After successfully downloading a catalog, the message Ready! appears in the dialog windows Check out catalog .