Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Note | |
---|---|
If PARTproject QA is activated, your catalogs are under SVN administration. In this case do not use PARTupdate! More information regarding PARTupdate can be found here: Abschnitt 1.1.3.3, „Katalogaktualisierung“. |
Within the project selection of PARTproject, it is not necessary that catalogs be managed by SVN. By means of the symbols mentioned above both states are well-defined.
Using PARTproject QA you are working exclusively with SVN managed catalogs.
For a local working basis you must download the catalog that should be used once. You will find 23d-libs in the context menu of the directory tree under the command Download catalog from server to do this.
The following screenshots show an example of the downloading of the catalog "maier".
In directory selects the desired catalog and confirms with OK.
After successfully downloading a catalog, the message Ready! appears in the dialog windows Check out catalog .
In PARTproject every catalog has to be set with General1 > Settings for the catalog, a QA-Status with value Yes, and a server path. Copy the path from the login dialog. |
|
Note | |
---|---|
If the option Update index after downloading catalog under Extras -> Settings... is set, the download time is extended. |