powered by CADENAS

Manual

Manual

6.9.3.2.6. Level 6

Coming from level 6 following QA levels can be set:

Set QA status

1 - Not released yet

2 - Released for editing (by customer)

3 - In progress

5 - Passed automatic test

7 QA-validation by project leader.

The Editor has the following rights:

  1. He sets the status back to 1-3, because relevant data is missing or incorrect and he wants to send the project back to the customer or editor.

  2. He sets the status back to 5 to double check.

  3. He sets the status up to 7, because the project passed his quality check.