Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
How to set and edit Release Notes?
Section 6.14, “ Publish catalog ”In order to set new release notes (normally before publishing), do the following:
In order to edit or delete entries, put the cursor into the desired field.
Then click on to edit or on to delete.
Where are the Release Notes displayed?
Once the catalog itself is selected on the left side in the tree, in the Edit project window, on the Translation tabbed page the single notes are listed.
When you move the mouse over a line in the left column, a preview with the original terms appears.
Right-click into the cell with the desired translation target language.
-> The Translation dialog box opens.
On the left side you can select one of the already translated languages via tabbed page.
On the right side the target language is displayed. Set the cursor into the desired text block and edit the content. Switch to the HTML view tabbed page - if needed.
If you translate a target language, still without content, may be it is helpful to use the context menu commands Select All and Copy on the left side and to paste the content into the target language on the right side using the Paste command.
If you use the
SVN rights management, it is possible to only checkout the file releasenotes.xml
for
editing.
Information on translation in general is found under Section 4.7.2.1.13, “ Translation ”.