powered by CADENAS

Manual

Manual

5.13.10.5.4. Import of existing cable classifications

Normally, classification data of cables are not manually entered into PARTproject, but imported via scripting.

For this there are two options:

  1. Data import of EPLAN part.xml files for cables (via EPLAN edz files)

    With this method a validity of data is guaranteed through EPLAN.

  2. Data import based on a provided Excel template.

In the context of EPLAN data (1. point), of course, concerning cable data, only the possibilities of EPLAN can be used. However, this import offers a direct out-of-the-box solution without the need to modify existing data. Should there be a requirement to further cable definitions which fully exploit the existing classification system, the second solution would offer. Here, you have the possibility to respond to special demands.