powered by CADENAS

Manual

Manual

9.5.1.7.1. Properties

  • Name: The name of the rule has to be unique!

  • Selection field:

    • Forbid autom. build (X)

      ...excludes the part which is created by this rule from the automatic assembly build [89] through the user.

    • Admit autom. build (U)

      ...includes the part (which is created by this rule) in the automatic assembly build (by user).

    • Always build automatically (V)

      ...includes the part (which is created by this rule) in the automatic assembly build.

    [Note] Note

    The abbreviation in parentheses in the configurator area indicate the used setting in the list field under Properties.

  • Exclusive: If there are different parts assigned to one connection point you can define a certain part as „exclusive“. Consequence: As soon as this certain part is selected the others (alternatives) are not available anymore.



[89] Information to automatic assembly build in PARTdataManager is found under Section 3.1.20.1.5.4, “ Connect assemblies automatically ” in PARTsolutions / PARTcommunity4Enterprise - User manual.