Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Chapter 3. General rules -
CADENAS Design Manual (CDM)
3.10.
Automatic Classification of standardized
Parts
|
|
---|---|
Prev | Next |
When a new release CIP is generated via PARTproject also a scanner is running during this process in order to identify and classify all kind of standardized parts. Explicitly all NNs and NTs were checked whether they contain one of the below listed keywords followed by a number like “123”, etc.:
DIN, ISO, ANSI B, NF E, VDI, UNI, NAS, NASM, BSI, ASNA, JIS, CSN, STN, GOST, JB/T, NIHS
EN, SN, LN, AN, SN, BS, IS, KS, GB, PN, GB, MS, VG
Especially within the 2-digit keywords there is unfortunately a high rate of mistakes and wrong classifications, because e.g. „Rohrbogen 90°“ is recognized as a EN 90 (an "Euro Standard”). Wrong classifications like this can be sorted out by inserting a „NO“ into the filed Similar to standard parts (optional) in PARTproject tab General -> Similar to standard parts (optional). If a catalog has wrong classifications, it must be checked from time to time by the responsible Project Manager.