Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This command opens the window with the same name. Therein you can apply the "business cards" of the part table.
The syntax of the standard name shows up in the Headline of the PARTdataManager (see fog.) when opening the respective part. |
Correct syntax is important in this case. Always enter your information inside the set of quotation marks. If you also wish to include table values, attach these in the format. |
|
Dollar sign variable name point at actual description: e.g. 'hexagonal screw ISO 4016 - $DG.x$L.'
If you open the ID datawindow, expression NB= '' is already provided but can also be inserted with button NB=.
Insert IF function in conditions. For mode of operation, see Section 11.5.2.7, “ Attribute algorithms ”.
Insert ELSEIF function in the condition Functionality see Section 11.5.2.7, “ Attribute algorithms ”.
Via Check standard description you can have the expression (syntactic) checked for correctness.
In the example, the standard name does not contain an applied variable.
The entry in this field forms the part name in the directory tree of the PARTdataManager-Part selection. [54]
[54] Standard Number and Standard titlecan later be changed in the Brief Description field of PARTproject.