Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The "Box" element constructs wildcard elements in the sketch frame, in other words, it defines position and measurement of the therein contained elements.
Box can be parent element of "Grid" (see Section 8.4.4.4, “[ELEMENT_grid] to place several derivations ”) and "Derivation" (see Section 8.4.4.6, “[ELEMENT_derivation] for one single derivation”) element.
The"Box" element is declared with "ELEMENT_" followed by a unique identification of the element.
[ELEMENT_box1]
The following attributes are available:
Box is embedded into frame element. (See Section 8.4.4.9, “[ELEMENT_frame] Combine more elements in frame ”)
Gives alignment of the elements contains in the box. Currently only "center" possible.
[ELEMENT_box1] type=box parent=frame position_x=260 position_y=90 position_w=140 position_h=170