Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
CADENAS PARTdxfConverter is a tool for automatically converting 2-D drawings, e.g. from 2-D programs such as AutoCad © and Medusa © etc. which have already been saved in these programs as files in dxf format or for dxf catalogs and integration of these files in the CADENAS PARTsolutions standard part system.
In order to do this, you determine a start directory in which the *.dxf files to be converted are located. After you have selected these, the corresponding files are located in the File structure field. If you click on a *.dxf file with the mouse you will see a preview of the relevant 2-D part analogously.
The elements in the Preview field can be chosen with the cursor so that the related layer from the drawing is displayed immediately, highlighted in color, in the Line assignment field.
When you have determined the user-specific changes, you can assign a new Project name to the project file (*.prj) or you can accept the file name proposed by the program which has been taken automatically from the dxf file. In addition, you can assign view names which are used as the preview name in PARTviewer 's Variant field.
After you have made the individual edit steps, you can start conversion with the Start... button and generate the project file (*.prj).