Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In this section you can find details on the setting options of Table .
General: The general standard settings are found under Section 14.4.2, “General settings”. At tables there is the feature that the overflow pages can have another specification than the first page.
Overflow x / Overflow y: Table position in the overflow section
Overflow width / Overflow height: Dimensions of the table in the overflow mode
Column definition: The value
$_Columns.
is
already inserted by default.
|
BOM Table: Via this option you can display BOM list information in a table.
BOM fields: In the list field, activate the checkbox at columns to be displayed.
Physical table: Via this option you can display physical information such as Volume, Plane and Mass.
Physical fields: In the list field, activate the checkbox at columns to be displayed.
Header font: For the design of the font in the table header there are setting options such as Font (hereto compare the same point under Section 14.4.5, “ Text ”), Font size, Font color, bold, italics and underlined available.
Font: For the design of the font in the table body the same setting options are available.
You can determine the color code of a single color, but also two. Then the background color of the lines, in the table body, is alternating (compare following figure).
#C8C8C8,#FFFFFF
Border type: "Solid" is the default value. In the list field, you can select from a variety of further options such as "dotted" for example.
Insert horizontal line: If you are using this separate layout option, the settings under Border color, Border size and Border type are ignored.
Switch rows and columns: See Fig. „Rows, columns interchanged and with alternative table header“.
This option can be used together with Switch rows and columns.
| ||||
[a] without "$", "." labeling |