Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
If lines have been interchanged or are not available in the new version anymore, an automatic mapping cannot be performed. You can recognize this at the respective icon in the table and in the directory tree. In this case the single suggestions have to be checked and confirmed line-by-line.
Example: The lines 1 and 2 have been interchanged, line 3 is not contained in the new version anymore, line 4 is line 3 of the old version and line 5 is unchanged.
On the left side, select the lines one after another and on the right side, check the assigned line (blue arrow ).
If a line is correct, click on the icon Approve assignment .
If a line is not available in the new version anymore, click on the icon Revoke the mapping to this project .
If all mappings are correct, click on the button Verify all mappings .