Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Create an assembly configuration.
Therefor, in the dialog area Project selection, on directory level, click on the context menu command New project. Enter a name. In the list field, select the option "Assembly configuration.prj". Confirm with OK.
-> The configuration is created in the project selection area of PARTproject.
In the context menu of the assembly configuration, click on the command Open with PARTdataManager.
Enable the Configuration mode.
-> Thereby the commands in the Configurator menu are enabled. (Otherwise they are grayed out.)
In the Configurator menu, click on the command Show configurations and tables.
-> Now the docking window Configurator becomes visible. The single dockings are still empty.
A detailed continuous example can be found under Section 10.7, “Example 1- Create a system of rules ”.