The
conventional Sketcher Sketcher (conv.) should only be used for parts which were
created with PARTsolutions V7.x.
Color settings:
Set the colors for the
different display elements in the conventional 2-D Sketcher. By
clicking on the respective color button, a selection menu
opens, in which the currently set color can be changed (see
figure).
Show base points:
Base points are especially
helpful for circles and 3-point arcs. If you do not want
the Base points of the given sketch elements to be
displayed, deactivate the respective options.
Performance:
Show construction elements: All help elements noted in the
Sketcher can be shown/hidden here.
Automatic switching: The End point of a line
defined in the Create line window creates both
the Start point for the line to be connected to it, if this
option is activated.