Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Use feature based Sketcher for new sketches : If you want to use the feature based instead of the conventional 2-D Sketcher, deactivate this option field.
Note | |
---|---|
The conventional Sketcher Sketcher (conv.) should only be used for parts which were created with PARTsolutions V7.x. |
Start only one instance of PARTdesigner : If this option is activated, several PARTdesigner sessions can no longer be started simultaneously.
Put decimal place on number block : This option switches the comma key on your keyboard into the period key, in otherwise you click on the comma key, but a period gets written. This is of advantage since when writing decimals in PARTdesigner, only periods (3 .5mm) and not commas (3 ,5mm) are required.
You may color the display of a 3-D solid using different settings.
To do so, simply click into the respective color box and select the desired color. This then enables the feature Base rotate to be colored in pink (see figure).
As soon as the option Activate has been selected, the adjustable intervals are automatically saved. Enter the desired interval Timeframe in minutes.