Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
6.8.6.
Value ranges
6.8.6.4. Type "Value range variable" in combination with IF
condition (attribute algorithm)
|
|
---|---|
Prev | Next |
When using value range variables you can also use an Attribute algorithm in addition. A frequent application is the use of an IF condition, to make the value range conditional upon the value of a certain variable.
In the following example an attribute algorithm has been used for the variable L1:[60]
IF( FORM1 .EQ. 1) THEN L1 ='100,[1:6000]' ELSE L1 ='100,[1:2000]' ENDIF
If the variable FORM1 has the value 1, then the value range of L1 is from 1 to 6000 with a default value of 100, otherwise the value range is from 1 to 2000.
The figure shows the selected variable "L1" with Status "Attribute algorithm" in the Variable Manager.[61]
The variable FORM1 is a Variable with fixed values. Here in the example it has the value 1 or 2. On this variable, the condition is focused.
The variable L is defined as Value range variable. It references the variable L1, which contains the attribute algorithm (see above).