Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
User interface of the dialog box Edit ERP mapping
In the index tree you can see at a glance which projects have automatically been mapped (these do not show icons) and which projects have to be edited manually.
Project/directory/catalog contains at least one line which could not be assigned. The change has to be confirmed. Possibly the correct line can be manually
assigned via |
|
![]() |
Confirmed (regardless of whether assigned or removed) |
![]() |
This assignment has been confirmed by the modeler |
![]() |
This line is expired. This was confirmed by the editor |
When moving the mouse over the icons tooltips are displayed.
![]() |
The plus button is used at different places:
|
||||
![]() |
With this function you can create a listing of all value combinations. When clicking on the button at the beginning of a line, an empty dialog box Edit value range mappings opens.
In order for the assignments to be displayed in the dialog box, at first you have to call the context menu command of a single line or the button above the table to create the assignments for all lines.
You can find an example on how to work with this function under Section 5.9.3.11, “Resolved value range”. |
||||
![]() |
Generate algorithm matching the selected line and copy it to clipboard When clicking
on the icon the value range algorithm is generated for the
selected line. Now, when clicking on Add condition
|
||||
![]() |
The x button is used at several places:
|
||||
![]() |
|||||
![]() |
Open project: When clicking on the icon, the respective project is selected in PARTproject. | ||||
![]() |
Approve assignment: Confirms the assignment of the selected line.
|
||||
![]() |
Verify all mappings: Confirms all assignments of the loaded project.
In the tree you can also find the context menu command Verify all mappings. This command is available for each directory level.
|
||||
Show hidden columns |
If there are hidden lines or columns in a table, then these are displayed when activating this option.
|
||||
Close the dialog by clicking on (right below). In this case all changes performed up to now are saved. Don't use the x button; in so doing you would loose the changes you made. (When using the command Add ERP-Mapping... the mapping information is updated (not overridden). |