Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The name conventions is to be explained in detail using the example of a profile:
A connection point is needed in the center of the section and one in each hole. Compare Fig. „3 connection points each at start and end, 8 insertion lines at the ducts“.
The connection point in the center of the section is called start, the others are listed as start_a, start_b etc.
The same counts for the profile end.
Sideway connection points (insertion lines)
![]() |
Note |
---|---|
The sideways Connection points are created as Connection line. See Section 6.9.3.2.1.6, “Create Connection line ”.
|
The following image is an example of the name convention for the insertion lines on the side. Your basic sketch is located on the start plane of the profile.
Example of a complex name convention with many connection points and insertion lines and different proportions
The start/end connection points/insertion lines are now a letter combination of top/side and or bottom/side: