Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
The following explains the basic instructions for use:
Activate button with simple mouse-click.
--> The buttons' function is "hanging" on
to the cursor and the button is marked by a frame.
Move the cursor to the desired location in the sketch.
--> Depending on the selected command, the object snap (circular symbol) becomes visible.
Carry out the function of the buttons through simple mouse-clicks at the desired spot (e.g. Insert line).
Automatic object snap for activated commands : If you move the cursor in the immediate area of an end, middle or intersection point, these points will be surrounded by a small circle and thus identified as a construction help point.
To improve the overview, the individual function buttons are summarized in groups with similar functions. You can also move a button group.
Right-click into a toolbar and set or remove the checkmark at the desired toolbar.