Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the hinge_asmtpl.prj context menu, you can find the command Create assembly table project .
The Create assembly table dialog box appears. Select the project from the pull-down menu, which contains the table with which you want to control the assembly. In this example, it is HINGEDUMMY. |
|
So far as the table "hinge_dummy" has been adjusted, the Standard name is correct; otherwise assign a definite standard name to the assembly.
So that only the Assembly-Table-Project is visible in the PARTdataManager, and not the "intermediary steps" template and assembly configuration, hide these with Hide project in the context menu of the directory tree. You should also hide the dummy project this way.
You can now select both single part, wing and bolt and the Assembly-Table-Project "hinge" in the PARTdataManager.
The assembly can now be committed to the CAD system as an Assembly-Table-Project (as in the example below, two times with L=50 and 2 differing angularities).