Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
Apply the order number as Standard variable in the part.
![]() |
Note |
---|---|
When exporting the part into the CAD system later, the respective Standard variables are found in the CAD system, in the file properties. |
![]() |
Note |
---|---|
You can also transfer the Standard variable CNSORDERNO via CNS classification into the CAD system. On this see Section 4.9.2.2, “ Menu item Variables ” (Variable with order number). |
In order to insert the Standard variable CNSORDERNO into the table proceed as follows:
Click on the button Standard variables.
-> The respective dialog box opens.
Activate the variables, which you want to overtake and confirm with OK.
-> Now the respective Standard variables are displayed in the list.
Close the dialog box Variable Manager by clicking on Ok.
-> Now the respective Standard variables are displayed in the table.
Instead of applying Standard variables in the table, you can apply the same variables as Class variables.