Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
For Part selection in PARTdataManager, dimensionings are automatically created in 3D view and 2D derivation. When exporting the part, the 2D derivation is transferred to the CAD system.
During modelling process respective data is parametrically created in PARTdataManager in the dialog area Dimensions.
Horizontal, vertical and parallel dimensioning | Radial dimensioning | Angular dimensioning | Annotations / Position numbers for list of material |
|
|
|
|
|
|
|
|
Working area is the docking window Dimensions. It is subdivided in two dialog areas:
In the upper dialog area, all dimensionings are listed with their description (ideally identical to the variable name such as L, R, D, etc.), in the lower area, the particular parameters of the selected dimensioning.
When selecting a dimensioning, the respective view in the 3D view is marked in green, Start point and End point in red. Vice versa, when selecting a dimensioning in the 3D view, the respective line is marked on the right side.
As soon as all Mandatory parameters are set, the dimensioning is displayed in the 3D view.
As soon as all Mandatory parameters are set, the dimensioning is also displayed in the 2D derivation.
When selecting a dimensioning line, in the lower dialog area, all parameters of this dimensioning are listed, namely separated in Mandatory parameters, Optional parameters and 3D Parameter. Here, parameters can be set or changed. Changes become immediately visible in the 3D view (if the mandatory parameters are set).
You can find detailed information on the mandatory parameters in the single chapters of the dimensioning types. Detailed information on the optional parameters can be found in an own chapter Section 4.10.7, “ Optional parameters Details ”.
Value changes
are signalized, once at the parameter itself by an undo icon
(when clicking on the icon the change is
reversed) and once in the list of dimensionings by red bold
font.
The undo icon
is displayed, as long as the change has not yet been saved by clicking
on Save changes . After this undo is not possible anymore.
Above the listing of dimensionings the following buttons are shown:
-> A new dimensioning is added to the list. At first the Type HORIZONTAL is displayed. If needed, adjust the selection in the list field under "Type". You can adjust the Type anytime.
–> A copy of the dimensioning selected in the list is created.
–> The
selected dimensioning is removed from the list. However, not until
Save changes has been clicked, the deletion is complete
and there is no "Undo" anymore.
–>
Changes are saved in the file *.dim
.
As long
as you do not click on the button Save changes , at the ID line above and at each changed
parameter an icon
is displayed. Clicking on the icon you can
undo the respective action.
All gray (inactive) lines are hidden. Compare ???.
Possibly at first set the needed dimensioning points
Since the measuring points reference to dimensioning points/connection points, they must either already be available within the part or specifically set.
Connection points may be used just the same as Dimensioning points.
File for saving the dimensioning parameters
If there
is no file for saving the dimensioning parameters available yet,
in the project, a file same-named to the project *.dim
is automatically
created and the key CUSTOMDIMENSIONSV9
in the Assembly Configuration
project file (*asmcfg.prj), Assembly Template project file
(*asmsbl.prj) or Single Part project file (*.prj) points to
this *.dim
.
If a
file customdimensions.txt
still exists from earlier versions, it will be used further on and
data is read and saved from there.