Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This section explains the user interface at a glance and then shows a simple use case so that you can become familiar with the working method in principle.
The user interface is subdivided in the following areas:
Directory structure on the left side
At projects without icon an automatic mapping has been performed.
At projects with icon an automatic mapping could not be performed.
A final check
and confirmation has to be done in both cases.
On the right side, the dialog box Edit ERP mapping is subdivided in an upper and lower half.
Initial situation: A project has been assigned automatically. However, you want to assign another project.
Click on
Revoke the mapping to this project
.
The table of the assigned project on the right side is deleted.
-> The dialog box Search or select project opens.
Select the desired project and click on .
-> Another Target project is added.
At the
desired project, click on the blue arrow Map this project to the currently selected line.
-> The dialog box Select table line opens.
Select the desired line and confirm with . (The variable name changed from 'A' to 'D' is correct. The change has been automatically detected.)
-> In the right table, the desired project with the desired line is displayed (see following figure).
Repeat the procedure for all desired lines.
Confirm the
mappings by clicking on Verify all mappings.
At all project lines and in the tree, a green checkmark is displayed as a symbol for the confirmed mapping.