Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
By these fields you are able to create an external Bill of Material.
Command line: this is where you define the program ("notepad.exe" in the example) to be launched as the "platform" for your Bill of Material. The placeholder "$BOMFILE 1 addresses BOMFile 1 and "$BOMFILE 2 addresses BOMFile 2 etc.
BOMFile 1, BOMFile 2 or BOMFile 3: Enter the name of the file in which the lower set content (from the applied program) should be read out. In the example, it is the content of variable column standard name "NB".