Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
Each part-notation must contain the following parameters:
ID is only required, if a dimensioning serves as Base dimension for a chain dimensioning.
The description is shown in the above listing. Initially a description is automatically given, when creating a new dimensioning, which can be adjusted as desired.
When creating a new dimensioning HORIZONTAL is automatically displayed. Adjust selection in the list field to PART-ANNOTATION. You can change the type anytime.
At the desired 2D views, where the dimensioning shall be displayed, activate the checkbox.
The respective position number is placed close to the desired connection point.