Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
With the help of a small example the working when creating a new dimensioning shall be shown.
A horizontal dimensioning shall be created for the length of a bolt:
In PARTdataManager, in the Part view, load the part to be dimensioned.
Possibly
activate the Configuration mode .[26]
In PARTdataManager, open the dialog area Dimensions by clicking on the same-named command in the context menu of the toolbars.
-> The dialog is displayed as docking area. You can detach the area via drag and drop so that it is displayed as a single window.
-> Now the dimensioning points and connection points are displayed.
Make sure that dimensionings are displayed in the 3D view.
Therefor, in the toolbar of the 3D view, click on the button Show Dimensions.
Make sure that the connection points are displayed in the 3D view.
Therefor, in the toolbar Assembly, click on the button Show connection points.
Click on
the button Create new dimension .
-> In the upper dialog area a new line "AUTO"-... is added and below, under Mandatory parameters the Type HORIZONTAL is created by default. (In the example in hand this is correct. Otherwise adjust the selection in the list field.)
Under Mandatory parameters -> Views, select the desired 2D view(s), where the dimensioning has to be displayed. Here in the example Front+ Z.
Views which contain a dimensioning,
can be recognized in the 3D toolbar by a respective icon with
dimensioning lines .
Now determine the Start point of the dimensioning.
Call the context menu and select Use as ... -> Start point.
Repeat the same procedure for the End point.
In the list field of Position, select the value BBOX (Bounding box) and under Offset (BBOX) the value -DIST*12 (here in the example).
-> As soon as all Mandatory parameters are set, the dimensioning is shown in the 3D view.
If needed, you can modify Optional parameters (e.g. Text) or set (e.g. Arrow size).
A complete summary of all PARTdesigner expressions can be found under Section 15.1, “PARTdesigner-Expressions ”.
Once the
variable name is entered, the editing icon is displayed.
Later, the user can change the characteristic here. Compare Section 3.1.7.6.6, “Change characteristic via dimension labels ” in PARTsolutions / PARTcommunity4Enterprise - User manual.
Adjust the value for font size accordingly (here in the example "DIST").
The set dimensioning is also used for the 2D derivation.
When exporting to the CAD system the dimensioning is transferred as well.
[26] In some cases the Configuration mode has to be activated and PARTdataManager to be restarted, in order for the connection points and dimensioning points to become visible.