Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Click on the arrow in order to open the list field with the project types. Select the desired type from there.
By selecting a type, a specific selection of tabbed pages shows up. You can find an overview on this under Section 4.9.1, “Overview on tabbed pages ”.
Project type | Description | |
Classification Search | ||
...you are prompted later in PARTdataManager as to whether it is to be opened as a 2-D or 3D project |
||
...is later asked for in the PARTdataManager whether it should be opened as 2-D or 3D project. | ||
Assembly configuration | ||
Assembly template | ||
Project documentation |
*.doc, *.HTML and *.pdf files etc. are created in the form of a project |
|
Assembly table | ||
Directory | ||
Project on the basis of a PARTmedia file (a print catalog can be created from PARTsolutions parts with PARTmedia) |
||
Without geometry | ||
Assistant |
...starts the PARTsolutions Web Wizard, which enables alternative masks for part selection to be displayed. See Section 3.1.6.4.13, “ Web Assistant (provided by customer) ” in PARTsolutions / PARTcommunity4Enterprise - User manual. |
|
Search Assistant | ||
Filter Assistant |
Global filter assistant created by administration. See Section 3.1.6.4.12.3.2, “ Search filter assistant (provided by PARTsolutions administration) ” in PARTsolutions / PARTcommunity4Enterprise - User manual. |
|
Calculation Assistant |
Name of person that applied and/or is working on this project.
Basically you must enter the license key with which the respective folder (catalog) is secured against unauthorized access. On the highest level (for example: C:\Programs\partsolutions/23d-libs) this is not provided.
Short name (max. 16 characters) :
The number character used should be oriented to the character limit of the "receiving" CAD system, since the short term is transferred as part name to the CAD during export.
The short name must be unique and should preferably include the DIN number and the value of the variable "NENN" (represented with a placeholder) (e.g. “D1587_$NENN.”).
Row Label: ...is displayed highlighted in gray as the second column from the left in the table (see Fig. „ Row Label, characteristic attribute table, Preview “). This retains your overview as to what component attribute you are dealing with in the relevant row even when scrolling to the right (the columns with the important identification variables would be concealed).
Information on the use of (translatable) text in the Row Label is found under Section 6.8.5.2, “ Translation functions”.
Similar to standard parts (optional):
When cipping a catalog it is detected automatically, whether there are links to standards projects in NT, NN and NB. If this is the case, then the project is automatically assigned to the class of the found Standards project within the Standards classification.
A manual entry here in the field Similar to standard parts (optional) results in the same.
Projects classified in such a way are marked with the Standards icon in PARTdataManager.
When using an ERP integration directories and projects can be colored based on role definitions in addition.
Information on this is found under Section 4.12.2, “ Create and configure roles ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
The table file contains the Table, which you can see in the Part view of the PARTdataManager (see figure below). Set the respective file (*.tab, *.tac).
Preview is the Image displayed in Part selection in the PARTdataManager (see illustration above). Likewise, in the Links side you can see the Part view (see illustration below). Enter the corresponding file (*.pra, *.bmp).
Under Product information pages, the catalog manufacturer can provide additional information ( e.g. installation information, shop info, etc.) for his catalog in HTML format. This can either be linked to a web site or being stored in a directory within the project directory. Variables can also be used. The syntax is the same as with document variables.
https://de.wikipedia.org/w/index.php?search=$NB.
Information is displayed in PARTdataManager, in the Part view, respectively on a dedicated tabbed page. The view dynamically shows the respective row selection in table.
At the option Product information pages, click on .
-> The same-named dialog box is opened.
Click on and create the desired pages. With and you can edit and delete entries.
Under
Name enter
Info 1
and
under Address
https://de.wikipedia.org/w/index.php?search=$NB.
for example.
-> In PARTdataManager, the created pages are displayed.
Under Additional export formats, additional files (export formats) can be made available for the export (e.g. Revit [RFA = Revit Family Tables], EPLAN, DXF with special tool layers).[22]
Additional
files can be made available for the whole project, but also per row or
value range value by adding a placeholder in the form of $VARIABLENAME.
.
In the following you can a description on how to create the needed entries.
[22] When using the Q&S import required entries are automatically created. Information on Quick & Simple can be found under Section 4.18, “ Create catalogs - Quick&Simple”.