Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
![]() |
Note |
---|---|
For already
delivered catalogs, this command is not available. (No |
Creating document projects means placing different file formats, such as for example *.html, *.pdf, etc., under the "cover" of a *.prj file. In this ways such formats can be integrated into the directory of the PARTdataManager as individual projects.
Let us assume, for example that you want to integrate an html file as catalog help, then proceed as follows:
With the help of the Explorer, set the html file plus possibly a bmp icon with the same name in the desired PARTsolutions directory.
In PARTproject, mark the Destination directory for the document project and open the Create document project menu window via context menu command under Automation.
Click on the button New type , enter ".html" as document type and confirm by pressing the Enter key. --> The fields Description and Preview are activated.
If, as the
Description , you enter %fname%
, the "fname" of the
html file will show up later in the PARTdataManager both in the directory tree
as well as in the title of the preview.
In order to set the bitmap with the same name (in this case "cataloginfo.bmp") as the preview symbol in the PARTdataManager, make sure you use the wildcard "%fname%", which in this case must contain the ending ".bmp".
In PARTadmin, in the category Index administration update the index for the new created directory.
Perform a double-click on "cataloginfo.prj".
-> The html file opens and is integrated as new document project.