Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In order to create preview images in a batch run, do the following:
The following explains the setting options in detail:
The source directory is automatically given. Usually you need not change the field entries.
Via Browse you may adjust the path if desired.
Optionally you can integrate the subdirectories for the creation of the preview images.
No target directory is given for the internally used preview images.
The option is deactivated if Create preview images is activated.
To create preview images, you must activate this option.
In the list field, select the desired perspective for the preview images.
In the list field, define whether the batch run should grab onto project or directory level, or both.
This setting is irrelevant for the creation of preview images
Storage location of text file in which the export process is protocolled. Via Browse you can adjust the path.
In the list field, select for example the BMP format.
Once all settings have been made, click on .
![]() |
Note |
---|---|
Should the new preview image not show up immediately, go up to the next highest level and then return back to the changed project. |