powered by CADENAS

FAQ Options

FAQ Information

  • Updated: May 2, 2014
  • Views: 6,446 views

FAQ Categories

Categories:

FAQ Description

How can I select a CAD model?

Follow the steps listed below to reach your desired part:

  1. Make sure that your are in the dialog area 3D CAD CATALOGS.

  2. Select the Catalog.

    Note

    While browsing the directory levels, click on the logo/image or the link.
    With Back you reach the previous level.
    WithHome you reach the catalog selection at the highest level.

     

  3. After you have selected a catalog, you may now select the catalog language.

    Note

    Catalog language and language for the user interface can be set differently. 

  4. At directory level  select product groups as long as a concrete assembly  or concrete single part  has been specified.

  5. Choose an assembly or a single part.

  6. As soon as a concrete row has been determined, a 3D view and dimensional drawings are loaded under CAD model preview.

  7. Define the characteristic of the part, by clicking into the option button before the desired row.

    Note

    No value range fields will be shown in the variable view.
    As soon as you are located in the table view and a row has been selected, the generation of a CAD model is possible (only useful if there are no value range fields to be set).

  8. Variable view (possibly set value ranges)

    In order to reach the variable view, click on the part link or preview image.

    -> You can now see all variables in list form.

    In case value range fields are available - you will recognize this by the yellow-highlighted fields - use the arrow  button in order to open these fields and select the desired value and simply enter it directly into the input area (alternatively also possible using a slider).

100% users marked this FAQ as helpful.
|
Was this answer helpful?
1 vote