Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Font color: The standard font color in Admin mode is black.
In the following the individual icons are explained. Links lead you to detailed information - if available.
Icons | Meaning / Legend | Cause - Solution |
Directory / file is contained in the Display index, thus displayed in PARTdataManager. |
||
The directory / file is not contained in the display index. This symbol is displayed, e.g., if project files had been copied in the 23d-libs directory via Explorer or if in PARTproject new directories or projects had been created. |
||
Directories / files have been deleted, but the index is still there. The directories are still displayed in the PARTdataManager, however, they cannot be loaded. |
If the display in PARTdataManager is not wanted, then please deinstall the catalog or suppress the display. |
|
Hidden entries (directories or files) are not displayed in the PARTdataManager. In the PARTadmin index administration, they are displayed with gray symbol and red font color.
|
With the following context menu commands, the display can be controlled. Suppress appearance <-> Restore appearance The command is available for all main folders (Catalogs, My parts, Classifications, Classification 2.0, User data, Fingerprints, Analyses). |
|
Directories that are linked and physically located at a different place, are displayed with a blue folder symbol and link symbol. |
More information concerning working with links can be found under Section 5.8.2.1.3, “ New link ” in eCATALOGsolutions Manual. | |
![]() |
||
![]() |
Entry is being updated | The symbol shows up when the Update menu is pressed. |
Icons for full-text search index
Icons | Meaning / Legend | Action |
![]() |
As soon as LinkDB content or role settings changed, the LinkDB search index has to be created anew. You can find more details on this under Section 1.3.8.6.2, “Context menu commands in detail ”. |
|
![]() |
Icons | Meaning / Legend | Action | ||||
![]() |
No further actions are necessary. At delivered catalogs, normally the geometric search index is pregenerated. |
|||||
![]() |
After a software update the geometric search index can be updated via context menu command Geometrical search index -> Create/Update .
|
|||||
![]() |
Geometric search index available (including partial search) | Regard notes on creation of index. See Section 1.3.8.6.2.3, “ Geometrical search index for Partial search ”. | ||||
![]() |
When catalogs (e.g. own part catalogs), directories and projects have been added subsequently the geometric search index can be created via context menu command Geometrical search index -> Create/Update.
|
In PARTadmin, in the status bar, an icon signalizes, whether the index is locked.
If a green lock
icon is displayed, then PARTadmin can access the
index.
If a red lock
icon is displayed, then the index is locked.
At mouseover a tooltip is displayed, showing the responsible computer and application.