Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In dialog area Variants, you can optionally determine, if the accessory part shall be displayed for the whole project or only for certain rows.
In the
dialog area Variants, click
on the button New
.
Variable "A" with value 18 stated - The accessory part is only displayed in the PARTdataManager later, if in the source project, a row with "A=18" is selected.
In the column Variable, open the list field and select that variable, with whose value you want to perform the restriction.
In the column Value, open the list field and select the desired value.
Update the
index and open the part in PARTdataManager.
In the docking window Links, select the list field option Accessories.
For testing select a row with a variable value determined before. -> Accessory part is displayed.
Select a row with variable value not determined before. -> Accessory part is not displayed.
Alternatively you can determine desired rows directly in the table. Then an appropriate formula expression is automatically generated.
Click on
the button New from table
.
-> The dialog box Select lines is opened.
Select the desired table rows (Ctrl = several single, Shift = as block) and click on .
-> On the right, the created formula is displayed.[44]
IDNR.LE.4
Confirm with . Optionally, you can still adjust the formula before.
-> Now the created expression is displayed in the dialog area Variants.
Now under Links to parts, determine the desired accessory parts. For this, proceed as already described before.
[44] For the formula creation Fortran syntax is used. On this, please see under Section 15.2.1, “Fortran Syntax ”.