Lechler M20 Tank Cleaning Machine with Horizontal Mount in Action - Side View
This shows the cleaning power of Lechler's M20 Tank Cleaning Machine with a horizontal mount for cleaning long tanks. While the standard vertical version alone can clean tanks up to 50' in diameter, this video shows a side view of how the same machine with Lechler's special horizontal mount allows it to effectively clean long tanks, such as truck interiors or railcars. It does so by spraying a sufficient amount of water to both bulkheads, something the vertical version alone, or any competitive model, cannot do.
Posted September 17, 2013
click to rate