3D printing is an emerging technology that has the potential to be adopted by a lot of businesses given the proper scalability. Direct writing technology is a big part of 3D printing that allows people to produce designs on a 2D or 3D surface or material. Some of the usual materials used in 3D printing are rubber, sandstone, polymer, and even metals and alloys, depending on the 3D printer that is being used. More useful information on Writing Kings .
Some of the industries that use it now include the medical field, electronics and semi-conductors, package design, furniture and architects for prototyping, industrial designers, toys and other
manufacturing industries.
The technology cost used to inhibit its wide use, but now 3D printing technologies have become more accessible than ever. It used to be that for a prototype of a product or a material to be made, it had to be done by suppliers that had access to the equipment used to make these materials. And some prototypes even required a minimum number of units for them to be made because they were manufactured using commercial and industrial-grade equipment. Direct writing technology 3D printing has changed all this by allowing people to have more control over the design of their prototype which can be produced for even a single unit.
Prototyping using 3D Printing allows people to test their own products and present them to prospective investors without having to shell out a big amount of money in production. There have also been cases where 3D printing has benefited people greatly. In the medical field, for instance, prosthetics for disabled people are printed specifically for that person’s size and body shape, such as legs and arms. Some research facilities are now even working on bioprinting organs for research and medical surgery.
3D printing is an exciting and emerging new technology, allowing for many new possibilities. People are no longer restricted regarding production, and they can try out new designs that they have been meaning to put out into the world but haven’t been able to because of the costs of production. Aside from the industries and benefits mentioned, there is still a lot of untapped potential for direct writing technology in 3D printing, and who knows, it might not be that long until we see it become a staple in every office and home, comparable to the electronics and appliances we see today.
3D-Airway Printed Splint good article about 3D printing