Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
For the automatic assignment a process has to be created.
In the context menu of Workspace -> Processes -> Article Assignment, click on the command Add new process.
Click on the button Load predefined template and then on the template Dimension search.
By selection of the individual nodes the respective setting options are displayed.
-> The dialog box Number search options is opened.
In the dialog box Number search options, determine source and target catalog by clicking on the search button and confirm with .
-> On the left under Processes -> Article Assignment, the process name is displayed.
One after another select the individual nodes. Thereby the respective setting options are displayed. The respective selection is marked in yellow. In nodes marked in red mandatory settings still have to be performed. In green nodes optional settings are available. A complete green pipeline is ready to be executed.
Select Product Source. The source catalog (created from the CSV file) is already displayed.
Select the node Line Finder NENN and determine the attribute (field) for Dimension and Material with a click on the search button .
Click on the Start button to execute the pipeline.
-> In the docking window Performance a respective message is displayed.
Optionally, save the process. In this way you can call it anytime and use it again (possibly modified). Click on the respective icon .